Skip to main content
Visitor II
May 2, 2006
Question

TIM1 and TIM on STR712

  • May 2, 2006
  • 2 replies
  • 730 views
Posted on May 02, 2006 at 05:54

TIM1 and TIM on STR712

    This topic has been closed for replies.

    2 replies

    ludo98Author
    Visitor II
    April 28, 2006
    Posted on April 28, 2006 at 08:16

    Hello, i have a question about the TIM1 and TIM2 of STR712.

    i would like to produce a signal with the TIM1 and TIM2 configurated in PWMO mode.

    I would like the signal of the ouput of the timer TIM pin.

    10

    +-----+

    | |

    | |_______________

    <--------------------->

    255

    following my code:

    for PWM0 (TIM1) :

    GPIO_Config (GPIO1 , 1<<7, GPIO_AF_PP );

    TIM_Init ( TIM1 );

    TIM_PrescalerConfig ( TIM1,0x1 );

    TIM_PWMOModeConfig ( TIM1, 10, TIM_LOW, 255, TIM_HIGH );

    TIM_CounterConfig ( TIM1, TIM_START );

    the signal is output is the following:

    10

    +-----+

    | |

    | |_______________

    <--------------------->

    255

    for PWM1 (TIM2) :

    GPIO_Config (GPIO0 , 1<<13, GPIO_AF_PP );

    TIM_Init ( TIM2 );

    TIM_PrescalerConfig ( TIM2,0x1 );

    TIM_PWMOModeConfig ( TIM2, 10, TIM_LOW, 255, TIM_HIGH );

    TIM_CounterConfig ( TIM2, TIM_START );

    the signal is output is the following:

    10

    +-----+

    | |

    _______________| |

    <--------------------->

    255

    the signals are reversed. My question is it's Normal?

    Thanks

    Ludovic

    ludo98Author
    Visitor II
    May 2, 2006
    Posted on May 02, 2006 at 05:54

    hello,

    thanks for your answer. the problem has been resolved.: at the output of the TIM1 a component( transistor) inverse the signal. now i play an wav file with th TIM1 at 8Khz frequency but have a correct sound but it's a little metal. Have you some advice to reduce this phenomen ?

    thanks

    since regards

    Ludovic