if the TIM_InitTypeDef structure is used and the timer is initialized like: /* TIM1 Configuration in PWM Mode */ TIM_InitStructure.TIM_Mode = TIM_PWM; TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB; TIM_InitStructure.TIM_Prescaler = 0xFF; TIM_InitStructure.TIM_Pulse_Level_1 = TIM_HIGH; TIM_InitStructure.TIM_Period_Level = TIM_LOW; TIM_InitStructure.TIM_Pulse_Length_1 = 0x0001; TIM_InitStructure.TIM_Full_Period = 0x0001; TIM_Init (TIM1, &TIM_InitStructure); This does not work as the TIM_Init() function assigns: /* Set the Duty Cycle value */ if ( TIM_InitStruct->TIM_Pulse_Length_1 < 5 ) { TIM_InitStruct->TIM_Pulse_Length_1 = 4; } but leaves TIM_Full_Period as it is. hence, for any TIM_Pulse_Length_1 < 5 timer does not work Work around: comment the section which does the assignment
FYI this condition was fixed for pecision reasons. In fact, to garantee a 50% of pulse length we eliminate pulse length and period values less than 4. But, I agree that it is a limitation that's why we will take it into account in the next revision of library (v1.2). Think you and best regards, mirou