I'd like to transmit data with the dma. At the same time I'd like to receive data using the IRQ (see the init code of post UART DMA). Now I found that the rx irq is not asserted if I have the DMA enable for tx. Any suggestion? Have I to manage the rx with DMA IRQ ?
person involved in a similar issue :D I found the bug in my code! I didn't initialize the GPIOIN for pin 6. Now I configured pin 6 as Alternate1 (UART0_RX) and the irq works. In any case is a strange behavior! without the dma transfer enabled the rx irq is asserted! OK, ok.. the micro is new... but I'm becoming nearly crazy ;)
sorry to directly contact you but i am student and I got a report to do aboutr MCU. I have to compare ST, Philips, Atmel, OKI component integrating ARM7 cpu. Could you help me?? I will have few question regarding the I/O voltage or erasing time for the flash...I think simple question... Thank you!! Let me know if I can send you some email with question....I sent directly to the forum but I feel like nobody will reply soon... Ciao, Saxo