I've sent this Question to just another thread, because of the similar issue. Perhaps here is the right place. I have got TIM0-Int for 1ms regularly. It works for so long, I don't get an RX-Int. After running the Rx_IRQ-Handler, the Timer has the OCFA/OCAIE- bits are set, but the Int is never served. my 71x_vec.s has the history-date:;* 13/01/2006 : V3.1 Any Idea? Steffen
I work with the IAR-Compiler and the softwarelib history tag: 13/01/2006 : V3.1 The issue is: I get 1ms ticks regularly, until there is a UART-RX-IRQ. Thereafter, there is no TIM0-IRQ. If I single-step it works fine?! The first question, Can I stop the clock during break in C-Spy. When I single step through this lines: IRQHandler SUB lr,lr,#4 ; Update the link register SaveContext r0,r12 ; Save the workspace plus the current ; return address lr_ irq and spsr_irq. LDR lr, =ReturnAddress ; Read the return address. LDR r0, =EIC_base_addr LDR r1, =IVR_off_addr ADD pc,r0,r1 ; Branch to the IRQ handler. ReturnAddress: ; Clear pending bit in EIC (using the proper IPRx) LDR r0, =EIC_base_addr LDR r2, [r0, #CICR_off_addr] ; Get the IRQ channel number. MOV r3,#1 MOV r3,r3,LSL r2 STR r3,[r0, #IPR_off_addr] ; Clear the corresponding IPR bit. RestoreContext r0,r12 ; Restore the context and return to the... ; ...program execution. The EIC_IPR0_0 won't be reset on the line :STR r3... Is this right? My Config looks like: EIC_IRQChannelPriorityConfig(T0TIMI_IRQChannel, INT_PRIO_TIM0); // priority from 1 to 15 ( low to high) /* enables global IRQ handling of EIC */ EIC_IRQConfig(ENABLE); /* Enable Timer IRQ in interrupt controller */ EIC_IRQChannelConfig(T0TIMI_IRQChannel, ENABLE); /* Initialize the Timer 1 registers to reset values */ TIM_Init ( TIM0 ); /* Configure the Timer 1 Prescaler */ TIM_PrescalerConfig ( TIM0, 0x00 ); /* Enable the Output Compare interrupt for the Timer 1 */ TIM_ITConfig ( TIM0, TIM_OCA_IT, ENABLE ); /* configure and enable Timer 1 */ TIM_OCMPModeConfig ( TIM0, TIM_CHANNEL_A, 0xFFFF, TIM_TIMING, TIM_HIGH ); and the Int: void T0TIMI_IRQHandler(void) { GPIO2->PD |= BIT14; /*Clear the TIM1 interrupt flag Bit 14 OCFA */ TIM_FlagClear(TIM0, TIM_OCFA); /* set next time to generate an interrupt */ /* to achieve 1ms at 24Mhz input frequency */ /* the value is set to 24000 ticks */ TIM0->OCAR += 3000; OSTimer(); GPIO2->PD &= ~BIT14; } Hopefully, Steffen
it was my fault. The error was in the UART-Tx. The problem is with the TXHalfempty-Flag. It is set after Reset, though in the reference is stated: â—� TxHalfEmpty is activated when data is moved from UARTn_TxBUFR to the txshift register. I understood this wrong. regards, S.Netz
The statement in the reference manual (TxHalfEmpty is activated when data is moved from UARTn_TxBUFR to the txshift register.) this is regarding the interrupt corresponding to TxHalfEmptyIE (Transmitter buffer Half Empty Interrupt Enable) and not the TxHalfEmpty flag.
However , you have to refere to section (11.3.1 Transmission) instead and you can find details about the TxHalfEmpty flag. ''If the fifos are enabled, UARTn_SR(TxHalfEmpty) is set when the TxFIFO contains 8 or fewer characters. If the fifos are disabled, the TxHalfEmpty flag set when the TxFIFO is empty.'' and it is set after reset. Regards.