Skip to main content
Visitor II
February 22, 2008
Question

UART0 not working

  • February 22, 2008
  • 3 replies
  • 799 views
Posted on February 22, 2008 at 12:17

UART0 not working

    This topic has been closed for replies.

    3 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    Hi,

    Im new to the ARM cores and to ST micros. I have been able to get my CAN and I/O to work fine but I cant seem to get the UARTS to react at all. I set it up with out FIFO load the DR register and expect to see a frame on the pin but instead all I get is the FR register showing Tx buffer full and UART0 busy. I checked the clock gating and reset holds. Setup up the GPIO 3.0 for RXD and 3.1 for TXD. Its on a reva board and im using Raisonance tool chain. code is as follows:

    SCU->PRR1 |= 0x00020000; // release P3 reset

    SCU->PCGR1 |= 0x00020000; // clock gating P3

    SCU->GPIOIN[3] |= 0x00000001;

    GPIO3->DIR &= 0xFE; // Dir input on GPIO3 for pin 0

    SCU->GPIOOUT[3] |= 0x00000008

    GPIO3->DIR |= 0x02;

    // SETUP the UART0

    SCU->PRR1 |= 0x00000008; // release UART0 reset

    SCU->PCGR1 |= 0x00000008; // clock gating UART0

    UART0->CR = 0x0380;

    UART0->LCR = 0x0060;

    UART0->IBRD = 0x0138;

    UART0->FBRD = 0x20;

    UART0->ICR = 0x07FF;

    UART0->CR |= 0x0001;

    UART0->DR = 0x34;

    for(;;);

    Im sure it something simple but I can't seem to get my head around it.

    Ryan

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    Thanks I hope it works with the library and I will try it out today.

    But my real problem is with understanding what register I have forgot to initialize to get the UART0 to TX. Is there a way to turn on BRCLK from FMSTR I assume it defaults ON as Fmstr/2 as per the docs.

    Ryan

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:50

    The STR9 library may help you to start with STR9 device. In fact it contains an example for UART. Just update it accordingly to your hardware.

    http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=101#Firmware