Skip to main content
Visitor II
June 6, 2025
Solved

Unable to Read the Byte from EEPROM m9564

  • June 6, 2025
  • 1 reply
  • 349 views

Edited the post to follow the community guidelines. In next time please use </> button to paste your code. See this post.

Hello Experts,

I  am unable to read the byte of data from eeprom in particular address after written the data.
i am getting the response from eeprom through miso line while reading the status register and i have checked again by changing the status register values. I am using tc397 as master.

this is my code:

void EEPROM_Write_Byte(uint16 address,uint8 data)

{

EEPROM_Write_Enable();

uint8 txdata[4] = {0x02, (address >> ‌‌ & 0XFF, address & 0xFF, data}; /* WRITE command, MSB address, LSB address, one byte Data */

IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel,txdata,NULL,4);

Wait_UntilReady(); /* wait for write operation completion*/

waitTime(IfxStm_getTicksFromMilliseconds(BSP_DEFAULT_TIMER, 200)); /* Time Delay for 10 milli seconds */

}



void EEPROM_Write_Enable()

{

uint8 command = 0x06;

IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel, &command, NULL_PTR,1);

waitTime(IfxStm_getTicksFromMilliseconds(BSP_DEFAULT_TIMER, 30)); /* Time Delay for 10 milli seconds */

}

uint8 EEPROM_Readstatus(void)

{

uint8 txdata[2] = {0x05,0x00};

uint8 rxdata[2]={0};

IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel, txdata, rxdata, 2);

return rxdata[1];

}



void Wait_UntilReady(void)

{

while(EEPROM_Readstatus() & 0x01); /* Checking write in progress bit */

}

void EEPROM_Read_Byte(uint16 address)

{

uint8 cmd[3] = {0x03, (address >> ‌‌ & 0xFF, address & 0xFF}; /* READ command, MSB address, LSB address*/

uint8 rx_data[3] = {0};

IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel,cmd,rx_data,3);

//IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel,NULL,&rxdata,1);

}

 

 

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome @Erambabu, to the community!

    You asked this question some time ago, but if it's still relevant: there is no M9564, which EEPROM are you using exactly?

    If you mean the M95640, that is a normal SPI EEPROM that you want to address as QSPI, which of course cannot work.

    Regards
    /Peter

    1 reply

    Technical Moderator
    October 13, 2025

    Welcome @Erambabu, to the community!

    You asked this question some time ago, but if it's still relevant: there is no M9564, which EEPROM are you using exactly?

    If you mean the M95640, that is a normal SPI EEPROM that you want to address as QSPI, which of course cannot work.

    Regards
    /Peter