I am using the uPSD3212, and planning to have the primary flash as program space and the secondary as the data space. The primary flash is devided in to 4 sector of 16K and I am planning to stack them up from 0x0000 to 0xFFFF. The socondary flash is 16K and I am planning to have it as two banks of 8K each and Please tell me if this will work ok or not?