Skip to main content
Visitor II
October 23, 2005
Question

uPSD33xx VM reg

  • October 23, 2005
  • 2 replies
  • 603 views
Posted on October 23, 2005 at 12:19

uPSD33xx VM reg

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:08

    I had a rep tell me that the 3300 unit was easier to use for applications where you need to download new code to a unit in the field. He eluded to a change in the memory map logic that made this chip more flexable that the psd813F2 I was using.

    Can anyone confirm this? I have looked in the manual but on a quick scan see no difference between the VM reg of a standard PSD part and the uPSD3354D series

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:08

    So theres no truth to the claim that flash in program space can be programed? As in the original part, you must have the flash in data space to change it?