USART1 Receive Problem with STM32L072CZ
Hi,
I'm trying to read via USART1 the bytes generated by the GNSS module.
I'm developing on the discovery kit B-L072Z-LRWAN1 board (Discovery kit LoRa), where the TX and RX pins of the GNSS module are connected respectively to PA9 and PA10 of the STM32.
In my code, I read the bytes (one by one) sent by the GNSS module via HAL_UART_Receive function, as shown below.
The problem occurs when the mcu executes the third call to
HAL_UART_Receive(). In this case the STM32 remains blocked and does not respect the timeout set as parameter.
The GNSS module works properly, with a UART-USB converter I can correctly read the bytes generated by the module.
This is my code:
#define UART USART1
#define UART_TX_PIN GPIO_PIN_9
#define UART_RX_PIN
GPIO_PIN_10#define UART_GPIO_PORT
GPIOA#define UART_AF GPIO_AF4_USART1
#define UART_CLK_ENABLE() __USART1_CLK_ENABLE();
//Uart Handle
static UART_HandleTypeDef uartHandle;
void GNSS_Uart_IoInit(void);
/*!
* @brief Initializes the UART interface
* @param None
* @retval None
*/
UART_HandleTypeDef GNSS_Init(void)
{
//Enable clock
UART_CLK_ENABLE();
__HAL_RCC_USART1_CLK_ENABLE();
GNSS_Uart_IoInit();
uartHandle.Instance = UART;
uartHandle.Init.BaudRate = 9600;
uartHandle.Init.WordLength = UART_WORDLENGTH_8B;
uartHandle.Init.StopBits = UART_STOPBITS_1;
uartHandle.Init.Parity = UART_PARITY_NONE;
uartHandle.Init.Mode = UART_MODE_TX_RX;
uartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
if(HAL_UART_Init(&uartHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
if(HAL_UART_GetState(&uartHandle) != HAL_UART_STATE_READY)
Error_Handler();
return uartHandle;
}
/*!
* @brief Initializes the GPIO for UART interface
* @param None
* @retval None
*/
void GNSS_Uart_IoInit(void)
{
__GPIOA_CLK_ENABLE();
/**UART GPIO Configuration
PA9 ------> UART1_TX
PA10 ------> UART1_RX
*/
GPIO_InitTypeDef GPIO_InitStruct = {0};
//Set pin
GPIO_InitStruct.Pin = UART_TX_PIN|UART_RX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
GPIO_InitStruct.Alternate = UART_AF;
HAL_GPIO_Init(UART_GPIO_PORT, &GPIO_InitStruct);
}
void readData(void)
{
uint8_t buff[2];
if(HAL_UART_GetState(&uartHandle) == HAL_UART_STATE_READY)
{
HAL_UART_Receive(&uartHandle, buff, 1, 200);
PRINTF('R: %c \n\r', buff[0]);
}else
PRINTF('BUSY');
}
}
This is the main:
int main( void )
{
//STM32 HAL library initialization
HAL_Init();
//Configure the system clock
SystemClock_Config();
//Configure the debug mode
DBG_Init();
//Configure the hardware
HW_Init();
GNSS_Init();
//Configure the Lora Stack
lora_Init(&LoRaMainCallbacks, &LoRaParamInit);
//Main loop
while(1)
{
//Run the LoRa class A state machine
lora_fsm();
readData();
}
The PRINTF function allows the communication with the pc through the st-link.
Thanks.