Skip to main content
Visitor II
May 17, 2004
Question

Usb-example!!

  • May 17, 2004
  • 2 replies
  • 609 views
Posted on May 17, 2004 at 16:45

Usb-example!!

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:00

    Hi!

    I don't know if anybody have tried to compile the uPSD DK3200 USB-example! because it isn't possible to compile! to much source code for the supported DevKit DemoVersion of Keil C-Compiler! What about people which do not have a full version! Must i buy one???

    or are there other possibilities!

    Best regards

    DANIEL

    [ This message was edited by: daniel24 on 17-05-2004 16:15 ]
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:00

    The latest released (April 2004) version of the USB demo code is available at:

    http://www.st.com/stonline/products/families/memories/psm/soft_c2.htm

    It compiles to around 5.5K bytes. The zip file containing the demo code also includes the compiled image in a hex file. Using PSDsoft Express and FlashLink (included in the DK3200 kit), you can load the demo program (hex file) into the memory on the 32xx device on your DK3200 board and try it.

    [ This message was edited by: uPSD on 17-05-2004 20:16 ]