On the STR10 Eval schematics there is a USBUF01W6 filter/buffer on the USB lines. From a quick look at the parts datasheet it seems to be connected with the in and outs the wrong way around.
The datasheet in not wrong, but here it is a misunderstanding about In/Out. In terms of USB we talk about IN and OUT transferts The reference in USB is always the Host PC , so : OUT : Data from Host to Device IN : Data from Device to Host We can see that the PinOuts of the USBUF01W6 ( ST emi filter and line termination for USB Upstream ports) in datasheet are correct since STR71x device is a Full Speed one. D+ device connected to 6 / D+ Host connected to 1 D- device conncted to 4 / D- Host connected to 3 Cheers, [ This message was edited by: Rave on 06-08-2004 12:16 ]
Thanks for the reply, but I still don't quite get this.
I am looking at at using the EVAL board schematics to make a test board. Looking at the USBUF01W6 data sheet Fig A1 or A2, for a full speed connection, the function / peripheral side of D+ shows that it is connected to D4 (pin6) of the device. On the Eval schematics there is a Type B connector, the board is the function side of the link, and D+(DP) from the connector is connected to pin1(D1) of the USBUF01W6, shouldn't this be D4(pin6) side ?
You are right, It is a mistake on The Eval Board Shematics... But anyway I think that It is not a good reference to be adopted if you want to have a Full Device, In this case you should be able to manage the Pull-Up of D+ with a GPIO. Regards,