Skip to main content
Visitor II
May 31, 2005
Question

USB intterupt

  • May 31, 2005
  • 1 reply
  • 528 views
Posted on May 31, 2005 at 11:27

USB intterupt

    This topic has been closed for replies.

    1 reply

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:07

    I am starting new project with USB interafce.

    Fisrst step I have check all with ST sample and all work OK

    Second step I have write mi own code and after first test I have some questions:

    I start my application next I connect USB cable to PC.

    I also store the UISTA value for the first interrupt only:

    unsigned char flag = 0x00 ;

    unsigned char tmp = 0xFF ;

    USBIsr()

    {

    if (flag==0) {tmp = UISTA ; flag =1 }

    ....

    }

    Every 500ms I copy to SBUF the tmp value and I send to PC via serial port. (serial connection tested)

    The read value is 0x00 !! Why the vector interrupt start if UISTA = 0 ?

    thanks for help