Skip to main content
Visitor II
November 15, 2021
Question

USBLC6-4SC6 for EFT and lightning protection

  • November 15, 2021
  • 1 reply
  • 652 views

Hi,

Can USBLC6-4SC6 be used to protect an IO from EFT (IEC 61000-4-4) and lightning (IEC 61000-4-5)? I do not see any specification for these standards? Thanks.

Regards

Gordon

    This topic has been closed for replies.

    1 reply

    ST Employee
    November 18, 2021

    Hi,

    Regarding IEC 61000-4-5, USBLC6-4SC6 is able to withstand 5A with a 8/20 µs surge, this is specified on the Table 2.

    Best regards.

    Fabrice.