Viper26LN 400V to 24V
Hello,
I'am currently working on a implemented design out of the DesignStudio. The general purpose of the Viper26 in Buck Config is to supply another DCDC with 24V. Currently a load of 110 Ohm (Bleeder) Resistor is placed for testing purposes which results in a avg. I of around 180 mA. (peak at around 225mA) with 4400 µH Inductor.
Now the question: The circuitry works as expected up to about 180V. After this the circuit shuts down. I have tried several things including: reducing output voltage to 18V (overvoltage Vdd?), higher inductor values (lower ripple current), thermal measurement (case temp 40 °C) , changing comp network etc. The ton time at 170 V is still 3µs so no minimal ton time...
What could be the reason for this shutdown?
Thanks a lot in advance and all the best
Matthias Neuner