Skip to main content
Visitor II
August 16, 2016
Question

viper37 junction temperature

  • August 16, 2016
  • 3 replies
  • 858 views
Posted on August 16, 2016 at 18:44

How i calculation junction temperature in VIPER37HD/LD

and how the frequency(60k,115k hz) Affect on junction temperature?

    This topic has been closed for replies.

    3 replies

    ST Employee
    August 18, 2016
    Posted on August 18, 2016 at 14:56

    Hello,

    The junction temperature is given by the following formula:

    Tj = Pdiss • Rth_ja + Ta

           where:

           Ta = ambient temperature

           Rth_ja = junction-to-ambient thermal resistance (reported on datasheet, its value can be reduced providing adequate copper area around DRAIN pins) </p>

    Pdiss = Pbias + Pcond + Pswitch + PCAP is the power dissipated within the VIPer, in particular:

                 Pbias = VDD • IDD1 (bias losses)

                             where:

                             VDD = voltage of the VDD pin (depends on the voltage delivered by the auxiliary winding of the transformer);

                             IDD1 = VIPer consumption, in switching conditions (reported on datasheet)

                 Pcond = Rdson • Irmsp conduction losses

                             where:

                             Rdson = on resistance of the VIPer (reported on datasheet)

                             Irmsp = primary RMS current (depends on input/output conditions, primary inductance, reflected voltage)

    </p>

    Pswitch = (Vin + VR) • Ipk • Tc • fsw/3 switching losses is an approximate formula where

                              where:

                              Vin = input voltage

                              VR = reflected voltage

                              Tc = crossover time (the time during which, at turn-off, both DRAIN voltage and current are not zero), should be estimated and is in the range of some tens nsec

                              fsw = switching frequency

      Ipk = primary peak current

    PCAP = Cdrain_par • Vds2 • fsw/2

                              where:

                              Cdrain_par = sum of all the capacitance of the DRAIN node (MOSFET output cap, reported on datasheet, plus stray capacitances due to the transformer)

                              Vds = DRAIN voltage value at turn-on

    The components PCAP and Pswitch depends linearly on the switching frequency  

    From: biton.pini

    </span>

    </span>

    </span>

    Posted: Tuesday, August 16, 2016 6:44 PM

    Subject: viper37 junction temperature

    How i calculation junction temperature in VIPER37HD/LD

    and how the frequency(60k,115k hz) Affect on junction temperature?

    Visitor II
    August 19, 2016
    Posted on August 19, 2016 at 09:06

    thanks alot for your help

    Pcond = Rdson • Irmsp conduction losses

    you meant that  the current in Square ?

    and if you  explain more what exactly  Tc

    best regard

    pinhas

    ST Employee
    August 22, 2016
    Posted on August 22, 2016 at 10:12

    -Iprms

    is the root mean square of the primary current

    -Tc

    At the end of the MOSFETs ON time, the DRAIN current has reached its maximum, while the DRAIN voltage is zero, thus the product IDRAIN*VDRAIN = 0W

    Some time after turn on, IDRAIN will be 0 and VDRAIN will be Vin + VR, so again IDRAIN*VDRAIN = 0.

    But in between, since the switch is not ideal, there is a time interval Tc when both IDRAIN and VDRAIN are >0, and so their product results in power dissipation at turn off.