Skip to main content
Visitor II
June 7, 2021
Question

VND5160AJTR-E current sensing limit and output current limit

  • June 7, 2021
  • 0 replies
  • 487 views

The datasheet does not explicitly call out maximum current that can be monitored with the "current_sense" pins but it appears to be 1.5A. Does that imply that this is also maximum continuous per output current that the part is rated to? Or is it 3.8A - the minimum short circuit current? Thank you.

    This topic has been closed for replies.