Skip to main content
Visitor II
November 24, 2020
Question

VNI8200XP - SPI command activates valves only for <500ms.

  • November 24, 2020
  • 0 replies
  • 511 views

+24V Supply, 16-bit SPI, I send the proper bytes to activate valve 1-8, the proper LED(s) is activated as expected, but only for a short period, then it turns off. The driver responds with the correct byte, no errors, parity check is clean. WD_EN is pulled to Ground, Enable pin is high. Any ideas?

    This topic has been closed for replies.