Skip to main content
Visitor II
January 6, 2005
Question

wake up from WFI and keep awake ??

  • January 6, 2005
  • 3 replies
  • 750 views
Posted on January 06, 2005 at 01:20

wake up from WFI and keep awake ??

    This topic has been closed for replies.

    3 replies

    shinnlinAuthor
    Visitor II
    January 5, 2005
    Posted on January 05, 2005 at 11:35

    Is it possible to wake from WFI by an INT and then keep awake until next time resetting

    mailto:WFI@PRCCU_SMR

    again ?

    Or

    mailto:WFI@PRCCU_SMR

    will keep its value reset automatically after been reset once ? And it only wakes up when an interrupt occurs, then enters WFI again after this interrupt is served.

    If so, this limits many applications....

    I can't say this mcu is good for low power application anymore..... :(

    Visitor II
    January 5, 2005
    Posted on January 05, 2005 at 12:31

    Hi shinn,

    Yes of corse when the device is awakened from WFI mode by an

    interrupt request it keep awake until next time resetting WFI PRCCU_SMR bit again.

    The device still runing after this interrupt is served.

    Best Regards

    HICH :p

    shinnlinAuthor
    Visitor II
    January 6, 2005
    Posted on January 06, 2005 at 01:20

    Thank you, HICH !

    I'll try it then...