I'm trying (unsuccessfuly) to use WFI mode to reduce power consumption between interrupts. Program execution stops when I clear WFI bit in RCCU_SMR register, but current remains the same. Once interrupt is detected program execution resumes. I tried it with 2 eval boards - IAR (STR712FR2) and Hitex (STR710FZ2).
I'm powering the board from external power supply and measuring the total current drawn from the board, so it includes LEDs, RS232 and CAN drivers. I tried several MCLK/FCLK/PCLK combinations, here are some of the results: MCLK FCLK PCLK mA 32 32 32 80 32 16 16 71 16 16 16 58 16 8 8 54 8 8 8 47 Application I'm running is very similar with AN2100 application note ''STR71x power management''. I cannot get any current reduction with WFI mode (RCCU->SMR &=0xFE;), eventhough processor stops program execution until detects interrupt. Thanks.