Skip to main content
Visitor II
April 15, 2021
Solved

What is 3.3V Vref in this circuit design of A6986? Do I need to supply 3.3V to this pin?

  • April 15, 2021
  • 2 replies
  • 985 views

https://eds.st.com/dcdc/

I want 9-30V to 8V and I don't have any 3.3V voltage in my circuit. Is it okay if I don't connect anything here?

0693W000008zfhZQAQ.png 

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome, @LTunc.1​, at the community!

    The VREF pin is an output and can be used to supply external circuitry with a reference voltage of 3.3 V + -3%, max 5mA, as stated in the datasheet, table 4.

    So no, you don't need to apply a 3.3V voltage to this pin, you are not allowed to either.

    Good luck!

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    /Peter

    2 replies

    Technical Moderator
    April 15, 2021

    Welcome, @LTunc.1​, at the community!

    The VREF pin is an output and can be used to supply external circuitry with a reference voltage of 3.3 V + -3%, max 5mA, as stated in the datasheet, table 4.

    So no, you don't need to apply a 3.3V voltage to this pin, you are not allowed to either.

    Good luck!

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    /Peter

    LTunc.1Author
    Visitor II
    April 16, 2021

    Thanks Peter, you've helped me a lot.