Skip to main content
Visitor II
October 3, 2005
Question

What is the maximum frequency generated with timers ?

  • October 3, 2005
  • 2 replies
  • 694 views
Posted on October 03, 2005 at 08:39

What is the maximum frequency generated with timers ?

    This topic has been closed for replies.

    2 replies

    pchignonAuthor
    Visitor II
    October 3, 2005
    Posted on October 03, 2005 at 07:21

    Hello,

    I'll be pleased, if it is possible to use the timer to provide a 12Mhz clock. Is it possible? What is the maximum frequency? How to?

    Is there another mean to get a 12MHz clock?

    Thanks,

    Ludo

    Visitor II
    October 3, 2005
    Posted on October 03, 2005 at 08:39

    I dont think you could get 12Mhz from a timer. I could be wrong.

    Probably your best bet (Assuming a 48Mhz MCLK) is to use the CKOUT pin. But this means running the APB2 peripherals at 12Mhz also.