What is the reason to restart the VIPER38HD chip continuously?
Hi, STMicroelectronics teams,
We are working on a project that uses a lot of STMicroelectronics components like VIPER38HD so we used “eDesignSuite - Design, Circuit, and Simulation Tools�? from STMicroelectronics.
The input of our circuit is
IC
VIPER38HD
Topology
ISOLATED FLYBACK
Input
90 Vac - 265 Vac
Output 1
12 V (2 %) - 9.6 W
Output 2
12 V (2 %) - 2.4 W
Recommended design from “eDesignSuite - Design, Circuit and Simulation Tools�?
fig [1]
And as you see in the above fig [1] the used converter is VIPER38HD, and we ordered it with the other components according to the schematic given in fig [1]. After we ordered all components, we made the circuit using VIPER38HD but our circuit did not work and we did not receive desired output voltage wave for the drain pin. After checking Vdd Pin We got to know the chip is restarting continuously. So we check the feed bak pin signal and the control pin signal and their voltages. but they are in between the given range. So we could not understand what could be the reason for the viper38hd chip restart problem. We double-check the component and values but there is no error with that. We checked for short circuits and confirmed that there is no short circuit problem also.
We got the above wave for Vdd Pin And Vdrain pin.
We are looking forward to your helping to troubleshoot this circuit and make it work as expected as soon as possible.
Thank you.