Skip to main content
Visitor II
May 9, 2021
Question

What recommendation do I follow to avoid losing data retention in NOR flash memory M29W640FT?

  • May 9, 2021
  • 2 replies
  • 1139 views

doubt flash memory

    This topic has been closed for replies.

    2 replies

    Graduate II
    May 9, 2021

    Voltage and Temperature tend to play a role.

    Are you looking for suggestions about checking integrity, using ECC or deep-cycle erasing?

    What kind of data are you trying to store/protect?

    ÍStef.1Author
    Visitor II
    May 9, 2021

    I have two copies of a snes cartridge both use the NOR flash memory STM29W640FT and in that memory the firmware of the cartridge is recorded a copy is saved and I do not use it regularly but if the firmware is erased the cartridge does not work and I want to keep the file always saved in this NOR flash memory

    will the files be silently deleted in the future?

    Graduate II
    May 9, 2021

    The flash memory should retain content over many years, if you're losing data something else is likely wrong.

    With these type of NOR memories the array could be deep-cycled via Erase, Write All Zeros, Erase, Write New Content

    ÍStef.1Author
    Visitor II
    May 10, 2021

    I am not losing data and they are recorded in the NOR flash memory M29W640FT 70N6 i doubt How many years does this memory retain data at a temperature of 34ºC?