Skip to main content
Visitor II
March 3, 2025
Question

Where is the Linux 6.1 TPM driver for ST33KTPM2X?

  • March 3, 2025
  • 1 reply
  • 605 views

Hi,

I am doing the evaluation of ST33KTPM2X-i2c on my Linux v6.1.70 embedded system.

According to the 'Enabling TPM support in the Linux kernel from the version 6.1' from an5714-integrating-the-stsafetpm-trusted-platform-modules-with-linux-stmicroelectronics.pdf, :

From the version 6.1, the TPM support can be enabled with a short method, which is available in the [TCG-TPM-I2C-DRV] github in Section 1: Open-source software resources.

I understand the driver is available within the Linux v6.1 already. What I need to to is to enable the tpm_tis_i2c.c and add device node into my DTB. Done!

But when I looked into the source code of Linux v6.1 (mainline or https://github.com/raspberrypi/linux/blob/rpi-6.1.y/drivers/char/tpm/tpm_tis_i2c.c#L385), the driver is not presented there - where I expect something like: .compatible = "st,st33ktpm-i2c". Could you help me?

    This topic has been closed for replies.

    1 reply

    ST Employee
    March 29, 2025

    Hello @LeoRuan 

    This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

    Regards,

    Roger