Skip to main content
Visitor II
June 2, 2003
Question

writing to any location in SRAM

  • June 2, 2003
  • 2 replies
  • 553 views
Posted on June 02, 2003 at 15:29

writing to any location in SRAM

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:54

    Hi,

    We would like to know , '' how we can access the SRAM space 8K''

    If we want to update/ read those location...

    what should be the syteps to achieve that..

    Is there any application code which uses SRAM in IAP mode ....

    For more information:

    We have develo the IAP code for upsd323X. In this case our IAP code will be in seconday...& application is in primary page1/page2 using the swap bit of page register..

    Now if we want to program the primary using IAP mode.& the packet size wil be of 20 bytes only....In this case we waould like to palce that in SRAM space & once verified we would like to copy the same in Primary flash.

    So we would like to know...how to access SRAM location ....

    It's w/o page & not overlapping to any of the flash location.

    Can we directly access these location??& wite using

    mov dptr,#(SRAM_LOCATION)

    mov a,#0xd0 ;data

    MOVX @dptr,a ;writng to location in SRAM (in data space)

    ret

    Thanks,

    Eagerly waiting for reply

    Purvi
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:54

    Hello,

    Our USB example code also uses the uPSD's SRAM, you can download it from our website at:

    http://psmdev.st.com/dk3200.php

    (dk3200_dsn_2.zip). The procedures on how to access the SRAM described in Sreeram's email is correct.