X-NUCLEO-GNSS1A1 expansion board wrong GPS location
Hi,
I have two X-NUCLEO-GNSS1A1 expansion boards.
I powered on the first board, and connected to UART port. I can read GPS messages from the board. GPS location is good. (I got GPRMC and GPGGA, GPGLL, etc.) I don't know what I did. Somehow NMEA messages report zero gps locations (0.0 N, 0.0 E). the UTC time stamp seems good.
Then I replaced with the second board, it reports GPS position (somewhere in Italy). It shall report as in New York.
Is it required to setup or configure the GPS micro firmware? Or it needs to select which satellite to use? No clue. Hope someone can help.
Thank you,
David