STHV1600 custom waveform generation Hi all,I have been testing the STHV1600 evaluation module and want to generate a continuous wave (CW) that would change after some time. Currently, the STSW-IME014 GUI software seems to allow creating multiple CW patterns and assigning them to a specific channel, but it does not allow changing the patterns once they are set.I am currently testing with four channels, and three output levels (Vp, Vm and gnd). I am trying to make so that all 4 channels are outputting 1MHz, 50% duty cycle waveform CW1 for 1minute. Afterwards, a delay is introduced to the channels so that each channel outputs the same waveform, but with a 1/4 of a period delay: t_start_0 = 0 us, t_start_1 = 250us, t_start_2 = 500 us, t_start_3 = 750 ns. This secondary pattern should run for a minute as well and then repeat. Generally, I would like to generate multiple delay patterns, that change over time.Could someone advise me on whether this is possible through STSW-IME014 GUI?In case it is not possible through the