sthv800: verify if reading state is ok? Hi allwe are using a custom PCB with the STHV800 IC on it, in the past we've used it primarily as a pulser IC, not yet to take the reading signal into account. Now that we want to take a look at the echo, we don't see the expected echo when comparing with a STHV748 evaluation board we have laying around: the STHV748 nicely shows the returning echo, yet nothing shows on the sthv800.Is there a way to verify if the IC is in the correct mode? We checked the input signals (CW = 2.5V, INx_0 = 2.5V, INx_1 = 0V). Clamping before RX is approx 48us, afterwards 90us. Thanks already!GreetingsWouter