Anyone have success with programming the NUCLEO-H723ZGT variant with Arduino IDE?
I was wondering if anyone has any experience using the H723ZGT variant within Arduino IDE successfully?
I followed through a tutorial on adding it as a variant to be recognized by the Arduino IDE.
I am at the point where I can compile the "blink" example and upload it to the board. I see the RGB LED (LD4) blink red and green after programming and then stay a solid red. I am expecting to see LD2 blink at around 1Hz after programming but I do not see anything. I have tried various other simple test programs without any luck.
Is anyone able to help me out or point me in the right direction?