Bug Report: STM32F0xx_DFP 3.1.1 — Registers missing in System Viewer (Keil MDK 5.43a)
Hello ST Support Team,
I am reporting a regression issue with the latest STM32F0xx Device Family Pack (DFP) version 3.1.1 when used with Keil MDK 5.43a.
Problem Description:
Installation Issue: The DFP 3.1.1 often fails to install via the Pack Installer, showing validation errors or failing to resolve dependencies.
Missing Registers: Even when successfully installed, the System Viewer in Debug mode is empty. Peripheral registers (GPIO, RCC, etc.) do not appear for the STM32F030 series.
Environment:
IDE: Keil uVision v5.43a.0
Device: STM32F030xx (all variants)
Pack: Keil::STM32F0xx_DFP.3.1.1
OS: Windows 11
Observations:
The issue seems to be related to the new SVD (System View Description) file structure or pathing in the 3.x.x branch.
Manually pointing to an older SVD file (from DFP v2.2.3) restores the register visibility.
The "System Viewer" list in the "Peripherals" menu remains blank when using the default settings of the 3.1.1 pack.
Request:
Please verify the compatibility of the SVD files in the 3.1.1 pack with the classic Keil uVision debugger interface and check for possible pathing errors in the .pdsc file.
Best regards,
[Kent]