External Mode with STM32L476RG not working
Hi all.
I'm trying to run external mode simulation using:
- Matlab R2022a.
- CubeMx 6.2.0
- STM32 Mat\Target(not sure which version)
- Nucleo L476RG
I have created a simple LED example to test the external mode and I used the Embedded Coder to integrate it with the CubMX Project file. The problem is when i'm trying to run in external mode, I can't do it because the Monitor&Tune button is grayed out and I can't press it. In the Hardware Implementation settings, I have checked the External Mode at the Interface section. Could you guys please help me where I went wrong?
Thanks a lot.