FDCAN H7 BRS failure with Kvaser Leaf 3
Heyho,
after some *** CAN beginner mistakes on my side, I got the FDCAN BRS 8 Mbit working.
Or so I thought. It's only working between my custom boards, as I found out after connecting a Kvaser Leaf v3.
With the Kvaser (directly connected to the board's D-sub, termination on, signals on the scope look good (enough)) and BRS on, it only works with max 2 Mbit, and only if the Kvaser's bit timing is set below 70% sampling point.
So far I played with changes to TDC, sampling point, SJW, and all bit timings (checked the Kvaser timing website).
Any ideas welcome!