Skip to main content
Visitor II
August 11, 2025
Question

Filter Circuit for USB , EEPROM and RS232 module

  • August 11, 2025
  • 3 replies
  • 300 views

hello  everyone ,
As i am trying to create a PCB project for my university project with stm32 MCU , at the moment i am kind of stuck in process of finding optimal filter circuit one needs to implement for optimal functioning , i have been reading through all the materials i can find and least to say there are many mixed suggestion and i also watched the stm webminar  and MOOC for USB but i am even more confused, 
so if any one can give me link for a  working project or just material that can help me implement my targetted components , any project that have implemented the suggested circuit will help
I am using M24M01 EEPROM , i want to add a USB-A port so that i can export saved files to USB thumbdrives and also add max232 module for serial communication 

3 replies

Technical Moderator
August 12, 2025

Hi @eva1000 

For USB type A implementation you can follow the schematics provided here

FBL_0-1754992162750.png

common-mode EMI filter and ESD protection are essential for robust connection and clean signals. For reference MB1939.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Andrew Neil
Super User
August 12, 2025

Check out ST's Application Notes; eg, 

AN4879: Introduction to USB hardware and PCB guidelines using STM32 MCUs

 


@eva1000 wrote:

 i am trying to create a PCB project for my university project with stm32 MCU 


What STM32, exactly?

For each family, you should find a Hardware Development guide; eg,

AN2586: Getting started with STM32F10xxx hardware development.

 

As @FBL suggested, check-out the schematics for ST's boards.

 


@eva1000 wrote:

 add max232 module for serial communication 


Is this a retro design project?!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
August 12, 2025

@eva1000 wrote:

 max232 module for serial communication 


The MAX232 is a 5V part - so not suitable for use with STM32.

Plenty of 3V alternatives are available ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.