FMC + LCD STM32H7S7L8 issue
Hello,
I'm working on a custom STM32H7S7L8 board with this display
https://newhavendisplay.com/fr/2-4-tft-lcd-ips-high-brightness-display/
Here the schematic of the connection in 8 bit mode and clock three


The backlight and display are working but I get a glitch image when i try to fill the display.

with this code i can see the display turning off and on so the command are working
Below the whole project zip
LCD_Fill(0xFFFF, 0, 0, 10, 10);
HAL_Delay(1000);
ST7789H2_DisplayOff();
LCD_Fill(0xFFFF, 0, 0, 10, 10);
HAL_Delay(1000);
ST7789H2_DisplayOn();
Does someone have a idea to make this work
Thanks