Has anybody tried using CubeMx v5.0.1, Windows 10, STM32 embedded target for MATLAB® and Simulink® release 4.4.2 and Matlab 2016b in their code generation examples?
I have tried using the examples to generate the code , but it seems it does not create an MDK-ARM project. I only see the Matlab generated files but no MDK-ARM project which I can flash directly to the device.
I was previously using Matlab 2015b, Windows 7, STM32 embedded target for MATLAB® and Simulink® release 4.1.1 and Cube Mx 4.7.1 and I have no problem generating the code from Matlab. Not quite sure if it is the Windows 10 causing the problem or something else.
Thanks!