hi, we are interfacing EEPROM to STM32L496ZG Nucleo board .but AT24C256 is failing to write data. Please find attached function to write data in EEPROM.We used A0 Device address to write data in EEPROM.Kindly Reply.
int at24_HAL_WriteBytes(I2C_HandleTypeDef *hi2c,uint16_t DevAddress,uint16_t MemAddress, uint8_t *pData,uint16_t TxBufferSize)
{
if(HAL_I2C_Mem_Write(hi2c,(uint16_t)DevAddress,(uint16_t)MemAddress,I2C_MEMADD_SIZE_8BIT,pData,(uint16_t)TxBufferSize,1000)== HAL_OK)
{
#if 1//TEST_DEBUG
sprintf((char *)&g_uc_Txbuffer[0],"\r\nS");
Fn_PutStr(g_uc_Txbuffer);
#endif//TEST_DEBUG
}
else
{
#if 1//TEST_DEBUG
sprintf((char *)&g_uc_Txbuffer[0],"\r\nE");
Fn_PutStr(g_uc_Txbuffer);
#endif//TEST_DEBUG
}
//if(HAL_I2C_IsDeviceReady(&hi2c1, 0xA0, 1, HAL_MAX_DELAY) == HAL_OK)
while(HAL_I2C_IsDeviceReady(hi2c, 0xA0, 1, HAL_MAX_DELAY) != HAL_OK);
//{
HAL_Delay(10);
if(HAL_I2C_Master_Transmit(hi2c, (uint16_t)DevAddress, (uint8_t) *pData, (uint8_t)TxBufferSize, HAL_MAX_DELAY)== HAL_OK)
{
#if 1//TEST_DEBUG
sprintf((char *)&g_uc_Txbuffer[0],"\r\nSW");
Fn_PutStr(g_uc_Txbuffer);
#endif//TEST_DEBUG
// return 1;
}
else
{
#if 1//TEST_DEBUG
sprintf((char *)&g_uc_Txbuffer[0],"\r\nError");
Fn_PutStr(g_uc_Txbuffer);
#endif//TEST_DEBUG
return 0;
}
}