How to use serial communication via the USB port on NUCLEO-H755ZI-Q by Arduino IDE
Hi, I'm new to STM32 and would like to know about serial communication
via the USB port on the NUCLEO-H755ZI-Q using Arduino IDE 2.3.6.
I've already tried the program below.
As a result, the LED (PB0) blinked, but I couldn't get serial communication with the PC to work.
Could anyone let me know how I can resolve this problem?
I apologize if the information is insufficient.
void setup() {
pinMode(PB0, OUTPUT);
Serial.begin(115200);
delay(2000);
Serial.println("START");
}
void loop() {
digitalWrite(PB0, HIGH);
Serial.println("LED ON");
delay(500);
digitalWrite(PB0, LOW);
Serial.println("LED OFF");
delay(500);
}
Settings on Arduino IDE
Debug symbols and core logs: "None"
Optimize: "Smallest (-Os default)"
Board part number: "Generic H755XIHx"
C Runtime Library: "Newlib Nano (default)"
Upload method: "STM32CubeProgrammer (SWD)"
USB support (if available): "None"
U(S)ART support: "Enabled (generic 'Serial')"
USB speed (if available): "Low/Full Speed"