Skip to main content
Senior
December 30, 2023
Question

I would like to use System Workbench but I can not find plug in for ECLIPSE IDE (STSW-STM32095)

  • December 30, 2023
  • 2 replies
  • 1808 views

Hi All,

I would like to use system workbench as I am having problem with STM32 CUBE IDE. In order to use system work bench, I need to have eclipse plug in installed, that is STSW-STM32095. I can see that this is obsolete. Could anyone please help me on this regard ?

Thanks.

2 replies

TDK
Super User
December 30, 2023

Download and install from here:

https://www.openstm32.org/HomePage

 

But why use that when STM32CubeIDE exists and is better in all aspects?

"If you feel a post has answered your question, please click ""Accept as Solution""."
demirAuthor
Senior
December 30, 2023

Thanks @TDK 

The link you've provided opens the download page for System Workbench, however I am looking for STSW-STM32095 plug-in which is required during system workbench to utilize STM32 Cube MX. Do you have that link with you ?

On the other hand, I have already create a thread about "STM32 CUBE IDE does not work on my machine", please see it here. If you could help me resolve that issue as well, it is more than welcome.

Thank you.

TDK
Super User
December 30, 2023

Ah, that makes a bit of sense. I never used the plugin. You can use STM32CubeMX in standalone mode and open the project it creates. Note that SW4STM32 is very similar to STM32CubeIDE, especially the debugging infrastructure, and you may end up running into the same issue.

Looked at the other thread. I have to believe it's a firewall issue. Looks like the debugger is trying to connect and can't. Hardware is fine since you can program in STM32CubeProgrammer. Although exit code -1 shouldn't be happening, so maybe your project wasn't created properly. Maybe make a new project to see if you can get it to build without error.

"If you feel a post has answered your question, please click ""Accept as Solution""."
demirAuthor
Senior
December 30, 2023

Thanks @TDK 

While waiting response from your end, I thought I should run the STM32 CUBE IDE with admin rights, and it worked! I can flash my code!!

I am getting below message when I run my code, does that mean anything to you ?

 

Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD]

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V2J43M28 (API v2) VID:PID 0483:374B

Info : Target voltage: 4.701055

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : clock speed 4000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x2ba01477

Info : [STM32F407VGTx.cpu] Cortex-M4 r0p1 processor detected

Info : [STM32F407VGTx.cpu] target has 6 breakpoints, 4 watchpoints

Info : starting gdb server for STM32F407VGTx.cpu on 3333

Info : Listening on port 3333 for gdb connections

Info : [STM32F407VGTx.cpu] external reset detected

Info : accepting 'gdb' connection on tcp/3333

[STM32F407VGTx.cpu] halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x08000c64 msp: 0x20020000

configuring PLL

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : device id = 0x100f6413

Info : flash size = 1024 KiB

Info : accepting 'gdb' connection on tcp/3333

[STM32F407VGTx.cpu] halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x08000c64 msp: 0x20020000

configuring PLL

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

[STM32F407VGTx.cpu] halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x08000c6c msp: 0x20020000

Info : dropped 'gdb' connection

[STM32F407VGTx.cpu] halted due to debug-request, current mode: Thread

xPSR: 0x21000000 pc: 0x08000dcc msp: 0x2001ff78

shutdown command invoked

Info : dropped 'gdb' connection