Associate II
December 9, 2025
Question
I2C NAK with SSD1317 oled display
- December 9, 2025
- 3 replies
- 719 views
Hello, i have a problem with I2C SSD1317 OLED display in combination with STM32. On arduino it works. On STM it works with other controllers but not with SSD1317. Display is working and address is ok (because it's working on Arduino). I tried different speeds and pullups.
Arduino and SSD1317:

STM32 and SSD1306:

STM32 and SSD1317:
Arduino code:
//Atmega88 SSD1317 OLED 4 pins I2C
//Buffer size 384Bytes
//Four 7 segment numbers are displayed. No flicker.
//Decimal point and frame graphics are provided.
//Without the character table, 30% of Flash and Ram are used only.
static byte bufr[384] = {};
unsigned long tim , bufridx ;
#define oled 0x3c
const byte initcode[]= { 0xae,0xd5,0x80,0xa8,0x2f,0xd3,0x00,0x40,0x8d,0x14,
0x20,0x00,0xa1,0xc8,0xda,0x12,0x81,0xcf,0xd9,0xf1, //0x81 contrast
0xdb,0x40,0xa4,0xa6,0x2e,0xaf};
void setup(void) {
TWSR=0x00;
TWBR=0x02; //8M / (16+2*2)*1 = 400khz
// Set pre-scalers (no pre-scaling)
//TWSR = 0;
// Set bit rate
//TWBR = ((F_CPU / TWI_FREQ) - 16) / 2;
// Enable TWI and interrupt
TWCR = (1 << TWIE) | (1 << TWEN);
//Serial.begin(9600);
//analogReference(INTERNAL);
//int n= analogRead(1);
for (byte j=0; j<sizeof(initcode); j++) { sendByte(initcode[j],0x00); }
fillRoundRect(0,0,21,21,5,1); displayon();delay(1000);
displayon();
drawCircle(15,35,10,1); displayon();delay(1000);wipe();
drawLine(0,0,5,47,1); drawLine(31,0,0,62,1);
displayon();delay(1000);wipe();
Move (0,0); Print("Boda "); displayon();delay(1000);wipe();
tim=millis();
}
void loop(void)
{ //static unsigned int c;
//numout(c++);
tim=millis();
for (int c=0; c<10000; c++) sendByte(0,0);
//Serial.print("Time ");Serial.println(millis()-tim);
//if (c>999) {c=0; Serial.print("Time ");Serial.println(millis()-tim); tim=millis(); }
}
// =============================== i2c routines =================================
void sendByte(byte DATA, byte mod ) //mod=0 control, 0x40 data
{
TWCR =(1<<TWINT)|(1<<TWSTA)|(1<<TWEN); //start condition
while (!(TWCR &(1<<TWINT))); //sent
//if ((TWSR & 0xF8) !=0x08) Serial.println("ERROR1");
TWDR = oled<<1 ; //address
TWCR = (1<<TWINT) |(1<<TWEN);
while (!(TWCR &(1<<TWINT))); //sent
//if ((TWSR & 0xF8) !=0x18) Serial.println("ERROR2");
TWDR = mod; //command or data
TWCR = (1<<TWINT) |(1<<TWEN); //sent
while (!(TWCR &(1<<TWINT)));
TWDR = DATA;
TWCR = (1<<TWINT)|(1<<TWEN);
while (!(TWCR &(1<<TWINT))); //sent
//if ((TWSR & 0xF8) !=0x28) Serial.println("ERROR3");
TWCR =(1<<TWINT)|(1<<TWEN)|(1<<TWSTO); //stop condition
}
void displayon(void) {
sendByte(0x21,0x00);sendByte(0x20,0);sendByte(0x20 + 64 - 1,0);
sendByte(0x22,0);sendByte(0,0); // Page start address
sendByte((48 / 8) - 1,0); // Page end address
for (uint16_t i=0; i<384; i++) sendByte(bufr[i],0x40);
}
#define swap(a, b) { int16_t t = a; a = b; b = t; }
void drawPixel(int16_t x, int16_t y, uint16_t color) {
//if (x>63 || y>47) return;
bufr[x+((y/8)<<6)] |= (1 << (y&7));
}
void clearDisplay(void) {
wipe();displayon();
}
void hLine(byte x, byte y, byte w, byte color) {
byte *pBuf = bufr;
pBuf += ((y/8)*64); pBuf += x;
byte mask = 1 << (y&7);
if (color) {while(w--) { *pBuf++ |= mask; };}
else {while(w--) { *pBuf++ &= ~mask; };}
}
void vLine(byte x, byte y, byte h, byte color) {
byte *pBuf = bufr;
pBuf += ((y/8) * 64); pBuf += x;
byte mod = y & 7;
if (mod) { mod = 8 - mod;
static byte premask[8] = {0x00, 0x80, 0xC0, 0xE0, 0xF0, 0xF8, 0xFC, 0xFE };
if( h < mod) premask[mod] &= (0XFF >> (mod-h));
if (color) *pBuf |= premask[mod]; else *pBuf &= ~premask[mod];
if(h<mod) return; h -= mod; pBuf += 64;
}
if(h >= 8) {
byte val =0 ; if (color) val = 255;
do {*pBuf = val; pBuf += 64; h -= 8;} while(h >= 8);
}
if(h) { mod = h & 7;
static byte postmask[8] = {0x00, 0x01, 0x03, 0x07, 0x0F, 0x1F, 0x3F, 0x7F };
if (color) *pBuf |= postmask[mod]; else *pBuf &= ~postmask[mod];
}
}
void wipe(void) {
//for (int h=0; h<=255; h++ ) bufr[h]=0;
memset(bufr, 0, 384);
}
void numout(unsigned int n){
if (n>9999) n=9999; //wipe();
hLine(0,0,64,1);hLine(0,47,64,1); vLine(0,1,47,1);vLine(63,1,47,1);
segment(n / 1000,0); n = n % 1000; segment(n / 100,1); n = n % 100;
segment(n /10,2); n = n % 10; segment(n,3); displayon();
}
void segment(byte c, byte pos) {
byte p15,n15; p15=pos*15;
if (c>9) c = 9;
const byte tab[]= {0x7e,0x30,0x6d,0x79,0x33,0x5b,0x5f,0x70,0x7f,0x7b};
const byte msk[]= {0x40,0x01,0x08,0x02,0x04,0x20,0x10};
byte color,js=3,xpos[]={3,18,33,48};
for (byte n=0; n<3 ; n++) { color = (msk[n] & tab[c]);
{ for (byte j=8; j<11; j++) hLine(3+pos*15,j+n*15,13,color); }
} fillRect(xpos[pos],8,2,35,0);fillRect(xpos[pos]+11,8,2,35,0);
for (byte n=0; n<2 ; n++) {
n15=n*15; if (msk[n+3] & tab[c]){
for (byte j=js; j<js+2; j++) { vLine(j+p15,8+n15,18,1); }} //seg f,e
if (msk[n+5] & tab[c]){
for (byte j=js; j<js+2; j++) { vLine(j+11+p15,8+n15,18,1);}} //seg b,c
}
}
void Move(byte x, byte y){
bufridx=y*64 +x;
}
void Print(const char *txt){
while (*txt) Cout(*txt++);
}
void Bcdout(unsigned int bcd)
{ unsigned int t5;
if (bcd>9999) bcd=9999;
for (t5=1000;t5>0;t5/=10) {Cout(0x30+bcd/t5); bcd%=t5;}
}
void Sgnout( int bcd)
{ unsigned int t5;
if (bcd<0) {Cout('-'); bcd=abs(bcd);} else Cout(32);
for (t5=1000;t5>0;t5/=10) {Cout(0x30+bcd/t5); bcd%=t5;}
}
void Bcd2( char bcd) {
if (bcd>9) Cout ((bcd/10) + 0x30); else Cout(32);
Cout ((bcd%10)+0x30);
}
void Hexout (unsigned char key){
unsigned char n;
n=(key/0x10)+0x30; if (n>0x39) n+=7; Cout(n); //convert to hex char
n=(key%0x10)+0x30; if (n>0x39) n+=7; Cout(n);
}
const PROGMEM byte Chartable[] =
{ 0x00 , 0x00 , 0x00 , 0x00 , 0x00, // Sp
0x00 , 0x00 , 0x2F , 0x00 , 0x00, // !
0x00 , 0x07 , 0x00 , 0x07 , 0x00, // ""
0x14 , 0x7F , 0x14 , 0x7F , 0x14, // #
0x24 , 0x2A , 0x7F , 0x2A , 0x12, // $
//0x7f , 0x7f , 0x7F , 0x7f , 0x7f, // $:full square
0x23 , 0x13 , 0x08 , 0x64 , 0x62, // %
0x36 , 0x49 , 0x55 , 0x22 , 0x50, // &
0x00 , 0x05 , 0x03 , 0x00 , 0x00, // '
0x00 , 0x1C , 0x22 , 0x41 , 0x00, // (
0x00 , 0x41 , 0x22 , 0x1C , 0x00, // )
0x14 , 0x08 , 0x3E , 0x08 , 0x14, // *
0x08 , 0x08 , 0x3E , 0x08 , 0x08, // +
0x00 , 0x00 , 0x50 , 0x30 , 0x00, // ,
0x10 , 0x10 , 0x10 , 0x10 , 0x10, // -
0x00 , 0x60 , 0x60 , 0x00 , 0x00, // .
0x20 , 0x10 , 0x08 , 0x04 , 0x02, // /
0x3E , 0x51 , 0x49 , 0x45 , 0x3E, // 0
0x00 , 0x42 , 0x7F , 0x40 , 0x00, // 1
0x42 , 0x61 , 0x51 , 0x49 , 0x46, // 2
0x21 , 0x41 , 0x45 , 0x4B , 0x31, // 3
0x18 , 0x14 , 0x12 , 0x7F , 0x10, // 4
0x27 , 0x45 , 0x45 , 0x45 , 0x39, // 5
0x3C , 0x4A , 0x49 , 0x49 , 0x30, // 6
0x01 , 0x71 , 0x09 , 0x05 , 0x03, // 7
0x36 , 0x49 , 0x49 , 0x49 , 0x36, // 8
0x06 , 0x49 , 0x49 , 0x29 , 0x1E, // 9
0x00 , 0x36 , 0x36 , 0x00 , 0x00, // :
0x00 , 0x56 , 0x36 , 0x00 , 0x00, // ;
0x08 , 0x14 , 0x22 , 0x41 , 0x00, // <
0x14 , 0x14 , 0x14 , 0x14 , 0x14, // =
0x00 , 0x41 , 0x22 , 0x14 , 0x08, // >
0x02 , 0x01 , 0x51 , 0x09 , 0x06, // ???
0x32 , 0x49 , 0x59 , 0x51 , 0x3E, // @
0x7E , 0x11 , 0x11 , 0x11 , 0x7E, // A UpperCase
0x7F , 0x49 , 0x49 , 0x49 , 0x36, // B
0x3E , 0x41 , 0x41 , 0x41 , 0x22, // C
0x7F , 0x41 , 0x41 , 0x22 , 0x1C, // D
0x7F , 0x49 , 0x49 , 0x49 , 0x41, // E
0x7F , 0x09 , 0x09 , 0x09 , 0x01, // F
0x3E , 0x41 , 0x49 , 0x49 , 0x7A, // G
0x7F , 0x08 , 0x08 , 0x08 , 0x7F, // H
0x00 , 0x41 , 0x7F , 0x41 , 0x00, // I
0x20 , 0x40 , 0x41 , 0x3F , 0x01, // J
0x7F , 0x08 , 0x14 , 0x22 , 0x41, // K
0x7F , 0x40 , 0x40 , 0x40 , 0x40, // L
0x7F , 0x02 , 0x0C , 0x02 , 0x7F, // M
0x7F , 0x04 , 0x08 , 0x10 , 0x7F, // N
0x3E , 0x41 , 0x41 , 0x41 , 0x3E, // O
0x7F , 0x09 , 0x09 , 0x09 , 0x06, // P
0x3E , 0x41 , 0x51 , 0x21 , 0x5E, // Q
0x7F , 0x09 , 0x19 , 0x29 , 0x46, // R
0x46 , 0x49 , 0x49 , 0x49 , 0x31, // S
0x01 , 0x01 , 0x7F , 0x01 , 0x01, // T
0x3F , 0x40 , 0x40 , 0x40 , 0x3F, // U
0x1F , 0x20 , 0x40 , 0x20 , 0x1F, // V
0x3F , 0x40 , 0x38 , 0x40 , 0x3F, // W
0x63 , 0x14 , 0x08 , 0x14 , 0x63, // X
0x07 , 0x08 , 0x70 , 0x08 , 0x07, // Y
0x61 , 0x51 , 0x49 , 0x45 , 0x43, // Z
0x00 , 0x7F , 0x41 , 0x41 , 0x00, // [
0x02 , 0x04 , 0x08 , 0x10 , 0x20, // Bksp
0x00 , 0x41 , 0x41 , 0x7F , 0x00, // ]
0x11 , 0x39 , 0x55 , 0x11 , 0x1F, // Lf
0x40 , 0x40 , 0x40 , 0x40 , 0x40, // _
0x10 , 0x38 , 0x54 , 0x10 , 0x1F, // Cr
0x20 , 0x54 , 0x54 , 0x54 , 0x78, // A LowerCase
0x7F , 0x48 , 0x44 , 0x44 , 0x38, // B
0x38 , 0x44 , 0x44 , 0x44 , 0x20, // C
0x38 , 0x44 , 0x44 , 0x48 , 0x7F, // D
0x38 , 0x54 , 0x54 , 0x54 , 0x18, // E
0x08 , 0x7E , 0x09 , 0x01 , 0x02, // F
0x0C , 0x52 , 0x52 , 0x52 , 0x3E, // G
0x7F , 0x08 , 0x04 , 0x04 , 0x78, // H
0x00 , 0x44 , 0x7D , 0x40 , 0x00, // I
0x20 , 0x40 , 0x44 , 0x3D , 0x00, // J
0x7F , 0x10 , 0x28 , 0x44 , 0x00, // K
0x00 , 0x41 , 0x7F , 0x40 , 0x00, // L
0x7C , 0x04 , 0x18 , 0x04 , 0x78, // M
0x7C , 0x08 , 0x04 , 0x04 , 0x78, // N
0x38 , 0x44 , 0x44 , 0x44 , 0x38, // O
0x7C , 0x14 , 0x14 , 0x14 , 0x08, // P
0x08 , 0x14 , 0x14 , 0x18 , 0x7C, // Q
0x7C , 0x08 , 0x04 , 0x04 , 0x08, // R
0x48 , 0x54 , 0x54 , 0x54 , 0x20, // S
0x04 , 0x3F , 0x44 , 0x40 , 0x20, // T
0x3C , 0x40 , 0x40 , 0x20 , 0x7C, // U
0x1C , 0x20 , 0x40 , 0x20 , 0x1C, // V
0x3C , 0x40 , 0x30 , 0x40 , 0x3C, // W
0x44 , 0x28 , 0x10 , 0x28 , 0x44, // X
0x0C , 0x50 , 0x50 , 0x50 , 0x3C, // Y
0x44 , 0x64 , 0x54 , 0x4C , 0x44, // Z
0x11 , 0x39 , 0x55 , 0x11 , 0x1F, // Lf
0x10 , 0x38 , 0x54 , 0x10 , 0x1F, // Cr
0x20 , 0x54 , 0x57 , 0x54 , 0x78, // A'
0x38 , 0x54 , 0x57 , 0x54 , 0x18, // E'
0x00 , 0x48 , 0x7B , 0x40 , 0x00, // I'
0x38 , 0x44 , 0x47 , 0x44 , 0x38, // O'
0x38 , 0x47 , 0x44 , 0x47 , 0x38, // O''
0x38 , 0x45 , 0x44 , 0x45 , 0x38, // O:
0x3C , 0x40 , 0x47 , 0x20 , 0x7C, // U'
0x3C , 0x47 , 0x40 , 0x27 , 0x7C, // U''
0x3C , 0x41 , 0x40 , 0x21 , 0x7C }; // U:
void Cout(byte Byte)
{ unsigned int t5;
for (byte t4 = 0; t4<= 4; t4++) {
t5 = Byte-32 ; t5 *= 5 ; t5 += t4;
bufr[bufridx++]= pgm_read_byte_near(Chartable + t5);
}
bufr[bufridx++]=0;
}
///////////////////////////////////////////////////////////////////////////
// Draw a circle outline
void drawCircle(int x0, int y0, int r, unsigned int color) {
int f = 1 - r, ddF_x = 1, ddF_y = -2 * r, x = 0, y = r;
drawPixel(x0 , y0+r, color);
drawPixel(x0 , y0-r, color);
drawPixel(x0+r, y0 , color);
drawPixel(x0-r, y0 , color);
while (x<y) {
if (f >= 0) {
y--;
ddF_y += 2;
f += ddF_y;
}
x++;
ddF_x += 2;
f += ddF_x;
drawPixel(x0 + x, y0 + y, color);
drawPixel(x0 - x, y0 + y, color);
drawPixel(x0 + x, y0 - y, color);
drawPixel(x0 - x, y0 - y, color);
drawPixel(x0 + y, y0 + x, color);
drawPixel(x0 - y, y0 + x, color);
drawPixel(x0 + y, y0 - x, color);
drawPixel(x0 - y, y0 - x, color);
}
}
void drawCircleHelper( int x0, int y0, int r, char cornername, unsigned int color) {
int f = 1 - r;
int ddF_x = 1;
int ddF_y = -2 * r;
int x = 0;
int y = r;
while (x<y) {
if (f >= 0) {
y--;
ddF_y += 2;
f += ddF_y;
}
x++;
ddF_x += 2;
f += ddF_x;
if (cornername & 0x4) {
drawPixel(x0 + x, y0 + y, color);
drawPixel(x0 + y, y0 + x, color);
}
if (cornername & 0x2) {
drawPixel(x0 + x, y0 - y, color);
drawPixel(x0 + y, y0 - x, color);
}
if (cornername & 0x8) {
drawPixel(x0 - y, y0 + x, color);
drawPixel(x0 - x, y0 + y, color);
}
if (cornername & 0x1) {
drawPixel(x0 - y, y0 - x, color);
drawPixel(x0 - x, y0 - y, color);
}
}
}
void fillCircle(int x0, int y0, int r,
unsigned int color) {
vLine(x0, y0-r, 2*r+1, color);
fillCircleHelper(x0, y0, r, 3, 0, color);
}
// Used to do circles and roundrects
void fillCircleHelper(int x0, int y0, int r,
char cornername, int delta, unsigned int color) {
int f = 1 - r;
int ddF_x = 1;
int ddF_y = -2 * r;
int x = 0;
int y = r;
while (x<y) {
if (f >= 0) {
y--;
ddF_y += 2;
f += ddF_y;
}
x++;
ddF_x += 2;
f += ddF_x;
if (cornername & 0x1) {
vLine(x0+x, y0-y, 2*y+1+delta, color);
vLine(x0+y, y0-x, 2*x+1+delta, color);
}
if (cornername & 0x2) {
vLine(x0-x, y0-y, 2*y+1+delta, color);
vLine(x0-y, y0-x, 2*x+1+delta, color);
}
}
}
// Bresenham's algorithm - thx wikpedia
void drawLine(int x0, int y0,
int x1, int y1,
unsigned int color) {
int dx, dy , err, ystep;
int steep = abs(y1 - y0) > abs(x1 - x0);
if (steep) {swap(x0, y0);swap(x1, y1);}
if (x0 > x1) {swap(x0, x1);swap(y0, y1);}
dx = x1 - x0;dy = abs(y1 - y0); err = dx / 2;
if (y0 < y1) {ystep = 1;}
else {ystep = -1;}
for (; x0<=x1; x0++) {
if (steep) {
drawPixel(y0, x0, color);
} else {
drawPixel(x0, y0, color);
}
err -= dy;
if (err < 0) {y0 += ystep;err += dx;}
}
}
// Draw a rectangle
void drawRect(int x, int y,
int w, int h,
unsigned int color) {
hLine(x, y, w, color);
hLine(x, y+h-1, w, color);
vLine(x, y, h, color);
vLine(x+w-1, y, h, color);
}
void fillRect(int x, int y, int w, int h,
unsigned int color) {
int i;
for ( i=x; i<x+w; i++) {
vLine(i, y, h, color);
}
}
// Draw a rounded rectangle
void drawRoundRect(int x, int y, int w,
int h, int r, unsigned int color) {
// smarter version
hLine(x+r , y , w-2*r, color); // Top
hLine(x+r , y+h-1, w-2*r, color); // Bottom
vLine(x , y+r , h-2*r, color); // Left
vLine(x+w-1, y+r , h-2*r, color); // Right
// draw four corners
drawCircleHelper(x+r , y+r , r, 1, color);
drawCircleHelper(x+w-r-1, y+r , r, 2, color);
drawCircleHelper(x+w-r-1, y+h-r-1, r, 4, color);
drawCircleHelper(x+r , y+h-r-1, r, 8, color);
}
// Fill a rounded rectangle
void fillRoundRect(int x, int y, int w,
int h, int r, unsigned int color) {
// smarter version
fillRect(x+r, y, w-2*r, h, color);
// draw four corners
fillCircleHelper(x+w-r-1, y+r, r, 1, h-2*r-1, color);
fillCircleHelper(x+r , y+r, r, 2, h-2*r-1, color);
}
// Draw a triangle
void drawTriangle(int x0, int y0,
int x1, int y1,
int x2, int y2, unsigned int color) {
drawLine(x0, y0, x1, y1, color);
drawLine(x1, y1, x2, y2, color);
drawLine(x2, y2, x0, y0, color);
}
// Fill a triangle
void fillTriangle ( int x0, int y0,
int x1, int y1,
int x2, int y2, unsigned int color) {
int a, b, y, last;
int dx01,dy01,dx02,dy02,dx12,dy12;
long sa,sb;
// Sort coordinates by Y order (y2 >= y1 >= y0)
if (y0 > y1) {swap(y0, y1); swap(x0, x1);}
if (y1 > y2) {swap(y2, y1); swap(x2, x1);}
if (y0 > y1) {swap(y0, y1); swap(x0, x1);}
if(y0 == y2) { // Handle awkward all-on-same-line case as its own thing
a = b = x0;
if(x1 < a) a = x1;
else if(x1 > b) b = x1;
if(x2 < a) a = x2;
else if(x2 > b) b = x2;
hLine(a, y0, b-a+1, color);
return;
}
dx01 = x1 - x0,dy01 = y1 - y0,dx02 = x2 - x0,dy02 = y2 - y0,
dx12 = x2 - x1,dy12 = y2 - y1;sa = 0, sb = 0;
// For upper part of triangle, find scanline crossings for segments
// 0-1 and 0-2. If y1=y2 (flat-bottomed triangle), the scanline y1
// is included here (and second loop will be skipped, avoiding a /0
// error there), otherwise scanline y1 is skipped here and handled
// in the second loop...which also avoids a /0 error here if y0=y1
// (flat-topped triangle).
if(y1 == y2) last = y1; // Include y1 scanline
else last = y1-1; // Skip it
for(y=y0; y<=last; y++) {
a = x0 + sa / dy01;
b = x0 + sb / dy02;
sa += dx01;
sb += dx02;
// longhand: a = x0 + (x1 - x0) * (y - y0) / (y1 - y0);
//b = x0 + (x2 - x0) * (y - y0) / (y2 - y0);
if(a > b) swap(a,b);
hLine(a, y, b-a+1, color);
}
// For lower part of triangle, find scanline crossings for segments
// 0-2 and 1-2. This loop is skipped if y1=y2.
sa = dx12 * (y - y1);
sb = dx02 * (y - y0);
for(; y<=y2; y++) {
a = x1 + sa / dy12;
b = x0 + sb / dy02;
sa += dx12;
sb += dx02;
// longhand: a = x1 + (x2 - x1) * (y - y1) / (y2 - y1);
// b = x0 + (x2 - x0) * (y - y0) / (y2 - y0);
if(a > b) swap(a,b);
hLine(a, y, b-a+1, color);
}
}