Issue with MIPI DSI Video Mode and SN65DSI83 Bridge on STM32H747
- March 27, 2026
- 1 reply
- 181 views
Dear ST Community,
We are currently working on the STM32H747 controller using the MIPI DSI interface in video mode.
In our setup, we are using the SN65DSI83TPAPRQ1 bridge to convert MIPI DSI signals into LVDS signals for our display panel.
The MIPI configuration and bridge configuration details are attached below.
After configuring the CSR registers on the bridge side, we are reading Register 0x0A and Register 0xE5 for status verification, as specified in the SN65DSI83TPAPRQ1 datasheet initialization sequence.
We have also enabled the test pattern, and the display turns ON (screenshot attached below).
Observations:
For Register 0x0A, bit 7 is not reading as 1
For Register 0xE5, the expected value is 0x00, but it is reading as 0x01
We are observing clock signals at the bridge output
However, no data signals are present on the LVDS side
Queries:
What could be the reason for bit 7 not being set in Register 0x0A?
What does Register 0xE5 reading 0x01 instead of 0x00 indicate?
Does this behaviour suggest an issue with DSI data lane activity or configuration?
Are there any additional requirements or configurations needed for DSI video mode on STM32H747 to ensure proper data transmission?
We kindly request you to review this and provide your guidance or debugging suggestions.
Thank you for your support.
Best regards,
Siddu M.