MAT Target External mode error. Chapter 2
Hi,
I want to use matlab simulink to program a ST-Nucleo_F303RE board,
with Matlab Simulink 2019b ver.2 with and extensions, ST MAT/TARGET,
CubeMX newest version and SW4. (because CubeIDE it does not work)
As a first attempt, I followed the MAT / TARGET documentation to implement a simple source code generation.
More or less, that worked after several hours/days. Without this forum, I would have no success. Because, as always special error treatment knowledge is needed. I mean very special. For this read other posts, not from me.
Now I want to use the external mode, because I need it in the end.
I followed the MAT / TARGET documentation again, without success !
Then I looked at an example code, in the example ADC folder, I generate with the CubeMX software my new processor icon file and this example Simulink circuit.

Then as I thought so a TransportLayer: ext_comm error !
After several hours, I came up with the idea to select the rider times and back again.

A success. Again special error treatment knowledge is needed ! You must switch tcpip and again to serial to update MATLAB =) , yes.

After the error handling, however, a new problem. And i dont know the special error treatment knowledge.

And how i must write the version number in the Toolchain selector ?
I tryed but, i dont know how it works.

And if I gerneate the External Mode Code for standalone mode, SW4 geht this error messages.

I hope somebody can help me =)
Best Regards
Aaron