Skip to main content
Associate II
March 18, 2025
Question

Nucleo F767ZI - Led LD4 RED

  • March 18, 2025
  • 2 replies
  • 1107 views

Hi, 

I'm new to stm32 boards and I'm using it on platformIO with Arduino framework. 
I have problems with the led LD4 (st-link led).

- When I use the USB cable (JP3 jumper on U5V -> powering the board using usb) the power led LD6 is green but the LD4 is red. When I upload the code the LD4 blinks red and then stable red again once flash is completed and nothing happens (in the code I turn on/off led LD1 and print something).

- When I use external power (7.6V battery on VIN, JP3 jumper on VIN) the power led LD6 is green, the LD4 is green as well. Once I upload the code the LD4 blinks red and then stable red again once flash is completed and nothing happens.

- Also, I tried doing the same thing with framework STM32cube but no luck (same behaviour).

Could you help me, what am I doing wrong?

- This is my .ini file:

[env:nucleo_f767zi]
platform = ststm32
board = nucleo_f767zi
framework = arduino
upload_protocol = stlink
debug_tool = stlink
monitor_speed = 115200
build_flags =
-D USE_FULL_ASSERT
-D DEBUG
-D SERIAL_DEBUG
 
- This is the basic code used:

 

 

#include <Arduino.h>

#define LED_PIN PB0 // Default user LED (LD1)

void setup() {
 Serial.begin(115200);
 pinMode(LED_PIN, OUTPUT);
 Serial.println("Setup Complete");
}

void loop() {
 digitalWrite(LED_PIN, HIGH); // Turn LED on
 delay(500);
 digitalWrite(LED_PIN, LOW); // Turn LED off
 delay(500);
}

 


- This is the output after flashing:

Archiving .pio/build/nucleo_f767zi/libFrameworkArduino.a
Indexing .pio/build/nucleo_f767zi/libFrameworkArduino.a
Linking .pio/build/nucleo_f767zi/firmware.elf
Checking size .pio/build/nucleo_f767zi/firmware.elf
Advanced Memory Usage is available via "PlatformIO Home > Project Inspect"
RAM: [ ] 0.3% (used 1332 bytes from 524288 bytes)
Flash: [ ] 1.1% (used 23012 bytes from 2097152 bytes)
Configuring upload protocol...
AVAILABLE: blackmagic, cmsis-dap, jlink, mbed, stlink
CURRENT: upload_protocol = stlink
Uploading .pio/build/nucleo_f767zi/firmware.elf
xPack Open On-Chip Debugger 0.12.0-01004-g9ea7f3d64-dirty (2023-01-30-17:03)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
debug_level: 1

srst_only separate srst_nogate srst_open_drain connect_deassert_srst

[stm32f7x.cpu] halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x08004534 msp: 0x20080000
** Programming Started **
** Programming Finished **
** Verify Started **
** Verified OK **
** Resetting Target **
shutdown command invoked

 

2 replies

Andrew Neil
Super User
March 18, 2025

@Danilo_ wrote:

 with Arduino framework. 


For Arduino questions, you should go here:

https://www.stm32duino.com/

Or the Arduino forums

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Danilo_Author
Associate II
March 18, 2025

Hi Andrew, 

The problem arises even when I use stm32cube as framework. 
I don't think it's a frawework related issue. 
I'll post my question on the link recommend by you. 
Thanks!

mƎALLEm
Technical Moderator
March 18, 2025

Hello @Danilo_ and welcome to the community;

Since you are using an external power supply, I suggest you to refer to the UM1974 / Section 6.4 Power supply and power selection.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."