Question
Observing Jitters and incorrect rotation angle of the servo with STM32F401 timers
Hi,
I am using Tower Pro SG90 servo motor interfaced with STM32F401. Timer 2 is used for generating PWM and timer 5 is used for generating the delay. I tried multiple code changes by myself and also took help from internet, but the servo jitters a lot, gets heated and gives the incorrect angle. Can anybody check my code and help me out?
#include <stdlib.h>
#include <stdint.h>
#include <stm32f401xe.h>
/*************This structure defines the registers for general purpose timers 2 and 5*************/
typedef struct{
volatile uint32_t REG_CR1;
uint32_t RESERVED0[2];
volatile uint32_t REG_DIER;
volatile uint32_t REG_SR;
volatile uint32_t REG_EGR;
volatile uint32_t REG_CCMR1;
uint32_t RESERVED1[1];
volatile uint32_t REG_CCER;
volatile uint32_t REG_CNT;
volatile uint32_t REG_PSC;
volatile uint32_t REG_ARR;
uint32_t RESERVED2[1];
volatile uint32_t REG_CCR1;
uint32_t RESERVED3[8];
}TIM_REG_DEFINES;
/*************This structure defines the registers for GPIO*************/
typedef struct{
volatile uint32_t REG_MODER;
volatile uint32_t REG_OTYPER;
volatile uint32_t REG_OSPEEDR;
volatile uint32_t REG_PUPDR;
volatile uint32_t REG_IDR;
volatile uint32_t REG_ODR;
volatile uint32_t REG_BSRR;
volatile uint32_t REG_LCKR;
volatile uint32_t REG_AFR[2];
volatile uint32_t REG_BRR;
}GPIO_REG_DEFINES;
/*************This structure defines registers for RCC*************/
typedef struct{
uint32_t RESERVED0[12];
volatile uint32_t REG_AHB1_ENR;
volatile uint32_t REG_AHB2_ENR;
uint32_t RESERVED1[2];
volatile uint32_t REG_APB1_ENR;
volatile uint32_t REG_APB2_ENR;
uint32_t RESERVED2[18];
}RCC_REG_DEFINES;
/*************Important MACROS*************/
#define SERVO_PIN 0
#define REG_RCC ((RCC_REG_DEFINES *)0x40023800)
#define GPIO_A ((GPIO_REG_DEFINES *)0x40020000)
#define TIM_2 ((TIM_REG_DEFINES *)0x40000000)
#define TIM_5 ((TIM_REG_DEFINES *)0x40000C00)
/*************This function enables the clock to GPIOA, TIM2 AND TIM5*************/
void GPIOA_TIM2_TIM5_Enable(){
REG_RCC->REG_AHB1_ENR |= 1;
REG_RCC->REG_APB1_ENR |= 1;
REG_RCC->REG_APB1_ENR |= (1<<3);
}
/*************This function sets up GPIO Port A pin 0 in alternate function 1 mode*************/
void GPIO_Setup(){
GPIO_A->REG_MODER &= ~(0x3 << (2*SERVO_PIN));
GPIO_A->REG_MODER |= (0x2 << (2*SERVO_PIN));
GPIO_A->REG_AFR[0] &= ~(0xF << (4*SERVO_PIN));
GPIO_A->REG_AFR[0] |= (0x1 << (4*SERVO_PIN));
GPIO_A->REG_OTYPER &= ~(0x1);
}
void TIM5_Setup(){
TIM_5->REG_CR1 &= ~0x1; //Disable the timer
TIM_5->REG_PSC = 15;
TIM_5->REG_ARR = 0xFFFFFFFF;
TIM_5->REG_EGR |= 0x1; //Load the PSC, ARR value immediately
TIM_5->REG_CR1 |= 1;
}
void delay_ms(){
uint32_t start = TIM_5->REG_CNT;
uint32_t ticks = 300000;
while((uint32_t)(TIM_5->REG_CNT - start)<ticks);
}
/*************This function sets up timer 2 for output compare on channel 1 and PWM mode 1*************/
void TIM2_Setup(){
TIM_2->REG_CR1 &= ~(0x1); //Disable the timer
TIM_2->REG_CCER &= ~(0x1); //Output compare disabled
TIM_2->REG_PSC = 15; //Use 15 for 1us ticks
TIM_2->REG_ARR = 19999; //For 20ms period
TIM_2->REG_CNT = 0; //Timer count zero (safe)
TIM_2->REG_CCR1 = 999; //For -90 degree (initial)
TIM_2->REG_CR1 |= (0x1<<7); //ARP preload enable
TIM_2->REG_CCMR1 &= ~((0x7<<4)|(0x3)); //Configure channel 1 for output compare and clear OC1M[1:0] and OC
TIM_2->REG_CCMR1 |= (0x6<<4); //set the pwm mode to 1
TIM_2->REG_CCMR1 |= (0x1<<3); //Output compare preload enable
TIM_2->REG_EGR |= 1; //Load the PSC, ARR and CCR value immediately
TIM_2->REG_SR &= ~0x1; //Clear update flag
TIM_2->REG_CR1 |= 1; //start the timer
while(!(TIM_2->REG_SR & 1));
TIM_2->REG_SR &= ~0x1;
TIM_2->REG_CCER |= 0x1; //Output compare enabled
}
void set_ccr_ticks(uint32_t ccr_ticks){
while(!(TIM_2->REG_SR & 1));
TIM_2->REG_SR &= ~0x1;
TIM_2->REG_CCR1 = ccr_ticks;
}
int main(){
GPIOA_TIM2_TIM5_Enable(); //Enable the clock to GPIOA, TIM2 and TIM5
GPIO_Setup(); //Setup the GPIO port A Pin 0 in AF mode
TIM2_Setup(); //Timer 2 in OC mode, pwm mode 1 on channel 1
TIM5_Setup();
//delay_ms(); //200 ms delay for initial stability at 0 degree
while(1){
set_ccr_ticks(999); //CCR value corresponding to 90 degree
delay_ms(); //200 ms delay for proper rotation
set_ccr_ticks(1499); //CCR value corresponding to 0 degree
delay_ms(); //200 ms delay for proper rotation
}
}Thanks in advance,