Porting ST67W6 from Nucleo U575ZI to custom baord with U575CI fails
- March 18, 2026
- 2 replies
- 224 views
Hi,
I´m trying to migrate the example Application p2pServer (BLE) from the Nucleo board to a custom board with an STM32U575CI, but it fails initializing:
#### Welcome to ST67W6X BLE P2P Server Application #####<\n>
# build: 17:52:14 Mar 18 2026<\n>
--------------- Host info ---------------<\n>
Host FW Version: 1.2.0<\n>
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:340) sem_if_ready not received<\n>
[ERROR] [4000] [ST67W6XTask] (w61_at_common.c:375) sem_if_ready not received<\n>
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:312) Could not init Modem handler<\n>
[ERROR] [4000] [ST67W6XTask] (main_app.c:975) [ERROR] in W6X_Init API<\n>
[ERROR] [4000] [ST67W6XTask] (w6x_sys.c:115) W61 Init failed<\n>
[ERROR] [4000] [ST67W6XTask] (main_app.c:401) Failed to initialize ST67W6X Driver
Any idea what could be the problem?
Best
Achim