Problems with setup of STM32H753-EVAL2 Evaluation Board
I'm trying to get the STM32H753-EVAL board to work.
- The power supply unit is connected, the demo software runs fine
- The board is connected to my PC via an USB cable ... an ST-Link Virtual COM port is visible in the device manager.
- In STM32CubeMX I selected the STM32H753I-EVAL2 board and generated a project for the Keil environment.
- I can compile the generated sources without errors.
When I try to upload, I get the following error messages:
Load "MPC_EVAL \\ MPC_EVAL.axf"
Erase Done.
Programming done.
Contents mismatch at: 08000300H (Flash = FFH Required = 52H)!
Contents mismatch at: 08000301H (Flash = FFH Required = 07H)!
Contents mismatch at: 08000302H (Flash = FFH Required = 28H)!
...
Flashing doesn't seem to work ... what can I do?
I need help urgently!
Many greetings
recently