Question
PWM no ouput on PB6 using ide PlatformIO
I am not able to discover the error It should work but i do not have any pulse on PB6
CPU STM332F103C8T6 ide PlatformIO
#include <Arduino.h>
void setup() {
RCC->APB2ENR |= RCC_APB2ENR_IOPBEN; // Enable GPIOB clock
RCC->APB1ENR |= RCC_APB1ENR_TIM4EN; // Enable TIM4 clock
RCC->APB2ENR |= RCC_APB2ENR_AFIOEN; // Enable Alternate Function clock
GPIOB->CRL |= (0b0011 << (4 * 6)); // Set PB6 as Alternate function output Push-pull (TIM4_CH1)
TIM4->CR1 = TIM_CR1_CEN |TIM_CR1_ARPE; // Enable counter and auto-reload preload
TIM4->CR2 = 0;
TIM4->SMCR = 0; // No slave mode
TIM4->DIER = 0; // No interrupts
TIM4->EGR = 0; // No event generation
TIM4->CCMR1 = (0b110 << 4 ) | TIM_CCMR1_OC1PE; // PWM mode 1, preload enable
TIM4->CCMR2 = 0;
TIM4->CCER = TIM_CCER_CC1E ; // Enable output on channel 1
TIM4->PSC = 71; // Set prescaler to have 1MHz timer clock (72MHz/72=1MHz)
TIM4->ARR = 0x5000; // Set auto-reload value, period of the PWM signal
TIM4->DCR = 0; // No DMA
TIM4->CCR1 = 1000; // Set compare value for channel 1, duty cycle
}
void loop() {
delay(10);
}[env:genericSTM32F103C8]
platform = ststm32
board = genericSTM32F103C8
framework = arduino