Skip to main content
Associate II
January 15, 2026
Question

STM32 USB Audio Class – Windows WASAPI cannot open microphone stream (4 channels)

  • January 15, 2026
  • 1 reply
  • 314 views

Hello,

I am implementing a USB Audio Class 1.0 microphone on an STM32 (Full-Speed only).
The device enumerates correctly on Windows and appears as a 4-channel microphone in the Sound Control Panel, but no WASAPI-based application can open the input stream.

When using Audacity with WASAPI, the device exposes only 1–2 input channels and recording cannot be started.

For USB Audio Class 1.0 Full-Speed microphones on Windows, I have the following questions:

  1. Are Sampling Frequency Control requests (GET_CUR / SET_CUR) required even if the device supports only a fixed sample rate of 48 kHz?
  2. Is the presence of a Master Feature Unit (Volume and/or Mute control) required for Windows/WASAPI to successfully open the audio stream?
  3. Are there any mandatory class-specific control requests that must be implemented (i.e. must not be STALLed) to avoid WASAPI stream open failures?

Setup:

  • STM32 USB Device (FS)

  • UAC 1.0, Isochronous IN (microphone)

  • PCM, 48 kHz, 16 bit, 4 channels

  • Iso IN Endpoint: Adaptive

  • Windows 11

 

File with descriptor file is attached below. Thanks in advance!

1 reply

Technical Moderator
January 30, 2026

Hi @MannyMarc35 

Would you provide better details about the STM32H7 product you are using? Are you using reference board ( nucleo or eval board)? Are you using drivers and middleware from CubeH7?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
April 7, 2026

Hi FBL 

 

You see? Same problem. I also got same issue  on STM32H743iitAudiosity.JPGAudiosity_1.JPG