STM32F407VG I2S slave mode and master clock question
Hello,
i'm starting a project with STM32F407VG and ADAU1466 DSP. The ADAU1466 generates the MCLK for the audio codec (ADAU1701), so far so good.
Now i'd like to implement full-duplex I2S communication between ADAU1466 and STM32 too using a different I2S port on the DSP. The idea is to set the STM32 as a slave receiver and let the DSP generate BCLK and LRCLK. In this context, do i need to provide master clock to STM32 too and if so, how? I mean, which pin should i use? For I2S2 i can see PC9 alternate function I2S_CKIN but i'm not sure if this is the proper way to provide external master clock.