Skip to main content
Associate II
April 7, 2025
Solved

STM32L0 Problem with EXTI handler on platform.io & arduino framework

  • April 7, 2025
  • 1 reply
  • 868 views

Hi,

 

I'm using a STM32L031K6 with platform.io & arduino framework. I know this forum is not relevant to platform.io or arduino, but most of my code is with LL drivers which should change nothing (but maybe ?).

 

First, i don't understand the IRQn. I'm using PB1 as input interrupt on rising, it's on line 1, so to start, it should be :

 
NVIC_EnableIRQ(EXTI0_1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
//as refered :
 EXTI0_1_IRQn = 5, /*!< EXTI Line 0 and 1 Interrupts 

But the interrupt work only if i enable EXTI2_3_IRQn. I don't get it, and in example EXTI_ToggleLedOnIT for NUCLEO-L073RZ, there is the same +1 on IRQn.

So, change made, and i can see the change of the interrupt on IEXTI->PR, depending on the rising on PB1. the problem is the call back function. On STM32 IDE, there is a *_it.h/c which don't exist on platform.io. Maybe the point come here.

First, i wanted to change the function handler using :

void IRQ_Module_0(void) {;}

NVIC_SetVector(EXTI2_3_IRQn, (uint32_t) &IRQ_Module_0);

But it seems to do nothing as the adress return by NVIC_GetVector stay the same. Or maybe i forgot something.

Second, i try to figure out with the defaut handler (which was hard to find, documentation is not clear) :

/**
 * @brief This function handles external line 2 to 3 interrupt request.
 * None
 * @retval None
 */
void EXTI2_3_IRQHandler(void)
{
 uint32_t pin;
 for (pin = GPIO_PIN_2; pin <= GPIO_PIN_3; pin = pin << 1) {
 HAL_GPIO_EXTI_IRQHandler(pin);
 }
}
// ->
void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)
{
 /* EXTI line interrupt detected */
 if (__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)
 {
 __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
 HAL_GPIO_EXTI_Callback(GPIO_Pin);
 }
}
// ->
__weak void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
 /* Prevent unused argument(s) compilation warning */
 UNUSED(GPIO_Pin);

 /* NOTE: This function Should not be modified, when the callback is needed,
 the HAL_GPIO_EXTI_Callback could be implemented in the user file
 */
}

with a new function :

extern "C" void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {;}

 And get an error :

test.cpp:(.text.HAL_GPIO_EXTI_Callback+0x0): multiple definition of `HAL_GPIO_EXTI_Callback'; .pio/build/nucleo_l031k6/SrcWrapper/src/stm32/interrupt.cpp.o:interrupt.cpp:(.text.HAL_GPIO_EXTI_Callback+0x0): first defined here

But it is defined as __weak

There is also in interrupt.cpp some :

void EXTI0_IRQHandler(void)
{
 HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);
}

 Finally, i'm totally lost. Did i make some missunderstanding ? Or maybe it is relative to platform.io ?

I search for some same error and didn't find it.

Some help would be appreciate.

Thx in advance,

Best answer by Frog

So, i add __weak to EXTI0_1_IRQHandler and EXTI1_2_IRQHandler inside framework-arduinoststm32\libraries\SrcWrapper\src\stm32\interrupt.cpp

It's dirty, but fastest way to solve it. I need to go to stmcube framework, but can't find a "all in one" LL (or HAL) printf library. Actually, i don't want to make my own.

Thanks,

1 reply

Andrew Neil
Super User
April 7, 2025

@Frog wrote:

I know this forum is not relevant to platform.io or arduino, ,


Indeed - maybe better to try here: https://www.stm32duino.com/

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
FrogAuthor
Associate II
April 7, 2025

In fact, there is a mistake cause of VSCode when i was looking to the function

__weak void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

Refer to the hal_gpio library, but in fact, it is declared inside interrupt.cpp

/**
 * @brief This function his called by the HAL if the IRQ is valid
 * @PAram GPIO_Pin : one of the gpio pin
 * @retval None
 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
 uint8_t irq_id = get_pin_id(GPIO_Pin);

 if (gpio_irq_conf[irq_id].callback != NULL) {
 gpio_irq_conf[irq_id].callback();
 }
}

 

But arduino framework or not, that change nothing about the EXTI2_3_IRQn for line1 and the problem of NVIC_SetVector which are from LL drivers

FrogAuthorBest answer
Associate II
April 7, 2025

So, i add __weak to EXTI0_1_IRQHandler and EXTI1_2_IRQHandler inside framework-arduinoststm32\libraries\SrcWrapper\src\stm32\interrupt.cpp

It's dirty, but fastest way to solve it. I need to go to stmcube framework, but can't find a "all in one" LL (or HAL) printf library. Actually, i don't want to make my own.

Thanks,