Skip to main content
SPand.25
Associate II
November 1, 2020
Question

Tera Term not working with STM32F407VG Board

  • November 1, 2020
  • 1 reply
  • 1160 views

I have been trying hard to produce a output in TeraTerm & RealTerm using uart2 via GPIO A Pins PA2 & PA3 which are directly connected to St-Linkv2 on my STM2F407VG Disc-1 Board. It just fails to produce anything. I am using STM32Cube IDE and STM32 CubeMX.

Pls Can Anyone help me out of this. I recently did the firmware upgrade to ST-LinkV2.1 and yes I got all the drivers installed already. I also did try to write my own main.c , msp.c and it.c ; still no output on TeraTerm.

Even I was facing the same issue when i tried STM32Duino, the Arduino Ide did not show any Serial output. Well that's for later, I want a solution to Stm32Cube Ide.

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_I2C1_Init();

 MX_I2S3_Init();

 MX_SPI1_Init();

 MX_USART2_UART_Init();

 MX_USB_HOST_Init();

 /* USER CODE BEGIN 2 */

 char* buf = "STM CORTEX M4 \r\n" ;

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  MX_USB_HOST_Process();

  HAL_UART_Transmit(&huart2, buf, strlen((char*)buf), HAL_MAX_DELAY);

  HAL_Delay(100);

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
November 1, 2020

The pins on the F4-DISCO are not wired to the VCP provided by the ST-LINK. You'd either need to wire them, or use a USB-To-CMOS Serial dongle

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..